NX Automatic Center Mark is not created while creating View in Drafting [NX11].

2021-10-06T23:26:17Z
NX for Design

Summary


Details

When creating the view in the drawing, even if you set the center line to be automatically created, the center mark is not created.
It is possible to manually create the center mark later.
User make a hole in the side of the cylinder and creating a center mark there. It is a spline as a line. He is able to create it without problems with NX 8 and NX 10.

Solution

The curve where Automatic Center Mark supposed to be created is not Circle/Arc - it's a Spline which projects as Arc.


After NX11 new settings is been provided to control the creation of Automatic Center Marks on such Splines. This can be found at Drafting -> preference -> view -> workflow -> Select Splines projected as Arcs -> Always.


Once this is turned ON then the Center Mark would be created on the required Spline.


Currently it's working as design.





Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V11.0
Function: ANNOTATION

Ref: 001-8978550

KB Article ID# PL8003830

Contents

SummaryDetails

Associated Components

Drafting